Sort by:

81 Results

SimpleLink™ Sub-1 GHz wireless solutions for the IoT: robustness & long range (3-part series)

Sub-1 GHz gives you kilometers of range with very low power consumption. The RF bands are license-free and the robust co-existence technology solves the increasing problem of interference from other wireless systems. Sub-1GHz is suited for applications running on small batteries: Metering and smart grid, alarm and security and home automation.

SimpleLink Wi-Fi CC3100 Project 0 Series

These videos support the software tool series for SimpleLink™ Wi-Fi CC3100:

  • SimpleLink™ Wi-Fi CC3100 Project 0: Energia IDE
  • SimpleLink™ Wi-Fi CC3100 Project 0: Microsoft Visual Studio
  • SimpleLink™ Wi-Fi CC3100 Project 0: IAR Embedded Workbench
  • SimpleLink™ Wi-Fi CC3100 Project 0: Code Composer Studio IDE

SimpleLink Wi-Fi CC3200 Project 0 Series

These videos support the software tool series for SimpleLink™ Wi-Fi CC3200

  • SimpleLink™ Wi-Fi CC3200 Project 0: Energia IDE
  • SimpleLink™ Wi-Fi CC3100 Project 0: IAR Embedded Workbench
  • SimpleLink™ Wi-Fi CC3100 Project 0: Code Composer Studio IDE

Use MSP432 microcontrollers to bring high performance to low-power applications

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity. Developers need to achieve higher performance within the same power footprint if battery life is not to be compromised.

SimpleLink Academy - Bluetooth low energy

SimpleLink™ Academy for Bluetooth® low energy CC2640R2 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC2640R2 Wireless MCU.

Getting Started with TI-RTOS Training Series

Getting started with TI-RTOS training series

The Getting Started with TI-RTOS workshop series, developed in association with Texas Instruments by Eric Wilbur and Scott Specker of

iOS/Android-Based Firmware Updates for SimpleLink Devices Training Series

This training series consists of everything a user needs to get started with updating the firmware running on their SimpleLink MSP432 device over BLE with a focus on the host side iOS and Android development. Technical details involving various components of mobile application development using BLE are covered copiously and reference applications for both iOS and Android are provided to users to use as a template for their designs.
Tech Days

Overview and Demos

Were you unable to attend Tech Day but want to view the featured content? Did you attend and want to revisit a particular session? This series contains many of the sessions from the embedded processing, power supply design, signal chain, and wireless connectivity tracks. In addition, this series features recordings of select TI demos from the exhibitors hall.

Tech Days

Wireless Connectivity

Were you unable to attend Tech Day but want to view the featured content? Did you attend and want to revisit a particular session? This series contains many of the sessions from the wireless connectivity tracks. In addition, this series features recordings of select TI demos from the exhibitors hall.

SimpleLink Academy for Sub-1 GHz

POSIX

The SimpleLink™ SDK features POSIX (Portable Operating System Interface), which is a family of standards specified by the IEEE Computer Society for maintaining compatibility between operating systems. Through POSIX-compliant APIs, developers can maintain 100% application code portability between various OS/kernels.

SimpleLink Academy for Sub-1 GHz

Proprietary RF

The CC13x0 wireless MCU features an integrated radio, which can be programmed to support various protocols. The CC1310 device features a sub-GHz RF radio, while the CC1350 device features a dual-band radio capable of both sub-GHz and 2.4GHz.

SimpleLink Academy for Sub-1 GHz

TI Drivers

The SimpleLink SDK includes TI Drivers, a robust set of intuitive, functional APIs that offer portable, feature-rich access to peripherals.  The TI Drivers API exposes the functionality of the hardware-specific drivers in the same way across all TI SimpleLink devices, giving developers portable, feature-rich access to a variety of peripherals. TI drivers are open source [Berkeley Software Distribution license (BSD)] and built on a hardware abstraction layer, offering full access to the device’s complete capability.

SimpleLink Academy for Sub-1 GHz

TI-15.4 Stack

The SimpleLink CC13x0 SDK includes the TI 15.4-Stack software, providing an IEEE 802.15.4e/g-based star topology networking solution for Sub-1 GHz band, along with a large set of proprietary RF examples for Sub-1 GHz based on the RF driver through the EasyLink RF abstraction layer.

SimpleLink Academy for Sub-1 GHz

TI-RTOS

The SimpleLink SDK comes integrated with TI-RTOS. Checkout the trainings below to learn about multi-threaded applications & the features available with TI-RTOS.

81 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki