Sort by:

79 Results
SimpleLink Academy for Sub-1 GHz

SimpleLink™ Academy for Sub-1 GHz CC13x0 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC13x0 Wireless MCUs.

SimpleLink Academy for MSP432

SimpleLink™ Academy for MSP432 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink MSP432 Host MCU.

SimpleLink Academy - Bluetooth low energy

SimpleLink™ Academy for Bluetooth® low energy CC2640R2 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC2640R2 Wireless MCU.

SimpleLink Academy for Wi-Fi

SimpleLink™ Academy for Wi-Fi® CC3x20 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC32x0 Wireless MCU.

Wireless Network Challenges and Solutions for a Smarter Grid IoT

The Internet of Things (IoT) is now part of the smarter grid through the adoption of IPv6 communications networks. These 6LoWPAN-based networks address key concerns such as standards-based interoperability, reliability, low power, and long-distance connectivity.

LC-sensing solution with TI FemtoFET and CC1350 Sensor Controller Engine

Single-chip Smart Water Meter with Dual-band RF and InfraRed port

Hundreds of millions mechanical water meters are deployed around the world today. Market pressure pushes water utilities to add intelligence and allow for automated readout and billing on top of water waste control. RF-enabled electronic flow measurement modules provide a cost-effective solution without full meter replacement and are the main building block for fully electronic smart water meters with impeller principle.

Introduction to SimpleLink SDK

Introduction to the SimpleLink SDK

Provides details of the software, hardware, tools, and resource components that make up the SimpleLink SDK software development kit, with an overview of TI-RTOS concepts and labs illustrating how to use the SDK to build and port applications between SimpleLink devices.

Bluetooth 5 Overview on the SimpleLink CC2640R2F wireless MCU

Introducing TI's fully qualified hardware and software solution for Bluetooth 5.

iOS/Android-Based Firmware Updates for SimpleLink Devices Training Series

This training series consists of everything a user needs to get started with updating the firmware running on their SimpleLink MSP432 device over BLE with a focus on the host side iOS and Android development. Technical details involving various components of mobile application development using BLE are covered copiously and reference applications for both iOS and Android are provided to users to use as a template for their designs.
SimpleLink Academy for Sub-1 GHz

POSIX

The SimpleLink™ SDK features POSIX (Portable Operating System Interface), which is a family of standards specified by the IEEE Computer Society for maintaining compatibility between operating systems. Through POSIX-compliant APIs, developers can maintain 100% application code portability between various OS/kernels.

SimpleLink Academy for Sub-1 GHz

Proprietary RF

The CC13x0 wireless MCU features an integrated radio, which can be programmed to support various protocols. The CC1310 device features a sub-GHz RF radio, while the CC1350 device features a dual-band radio capable of both sub-GHz and 2.4GHz.

SimpleLink Academy for Sub-1 GHz

TI Drivers

The SimpleLink SDK includes TI Drivers, a robust set of intuitive, functional APIs that offer portable, feature-rich access to peripherals.  The TI Drivers API exposes the functionality of the hardware-specific drivers in the same way across all TI SimpleLink devices, giving developers portable, feature-rich access to a variety of peripherals. TI drivers are open source [Berkeley Software Distribution license (BSD)] and built on a hardware abstraction layer, offering full access to the device’s complete capability.

SimpleLink Academy for Sub-1 GHz

TI-15.4 Stack

The SimpleLink CC13x0 SDK includes the TI 15.4-Stack software, providing an IEEE 802.15.4e/g-based star topology networking solution for Sub-1 GHz band, along with a large set of proprietary RF examples for Sub-1 GHz based on the RF driver through the EasyLink RF abstraction layer.

SimpleLink Academy for Sub-1 GHz

TI-RTOS

The SimpleLink SDK comes integrated with TI-RTOS. Checkout the trainings below to learn about multi-threaded applications & the features available with TI-RTOS.

79 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki