3.1 Power Tips: Measuring Vout Ripple in DC/DC Converters
描述
2017年 7月 13日
The video explains the measurement set-up for the output voltage ripple in DC/DC converters. It compares the oscilloscope measurement results using 20MHz bandwidth limitation to a full bandwidth measurement with high frequency bypass capacitor. It is important to verify the voltage ripple directly at the load where high frequency bypass capacitors are used. The video also demonstrates the forced PWM feature of the TPS62135 minimizing the output voltage ripple over the entire load current range. |
其他資訊
This course is also a part of the following series
Date: 九月21日2015年
Date: 九月23日2017年