登入/註冊
注意:各項之間請以逗號分隔
Date
例如 , 06/17/2022
Date
例如 , 06/17/2022
Taiwan (繁體中文)
Global
China (简体中文)
Japan (日本語)
Korea (한국어)
Taiwan (繁體中文)
TI training & videos >
Applications & designs
Live training
Products
Tools & software
Toggle navigation
注意:各項之間請以逗號分隔
Date
例如 , 06/17/2022
Date
例如 , 06/17/2022
Global
China (简体中文)
Japan (日本語)
Korea (한국어)
Taiwan (繁體中文)
TI Training home
RFID
RFID: LF Applications
RFID
電子郵件
RFID: LF Applications
Let's look at an overview of the application examples and associated form factors for LF. In the red boxes, you can see the application field. Blue boxes show the key care-abouts. For example, let's take livestock and pets. The most important factor here is reliability. The tags will need to stay on this cow for one, two, even five years sometimes. And it's also very important to get significant range on this tag. Again, reliability on the left photo, we can even see tags being injected into fish in order to tag and check their migration path upstream and whether this still works in case of a hydropower plant. The most prominent of these tags are air coil, copper wire, and antenna with a small, tiny chip or module. Glass encapsulated tags provide perfect reliability and hermetic sealing against water and chemicals. In the automotive field, security is a large factor in addition to reliability. What we see here is automotive immobilization. There are very tiny little tags molded into the car key, but also deliver state of the art security like AES cryptography. In the industrial field, we have reliability as a key requirement as well. And that's ensured by stable plastic encapsulated tags which can survive harsh environments. On the top right, you see waste management, and again, reliability is a key concern. We see tags in operation which have been out there for 10 or even 20 years and still functional. In this very harsh environment with tough requirements, the technology is more than well-suited to deliver that reliability. Moving on to sports, anyone who's been to a running marathon has seen the tag on the shoelace. On the access control side, we need security. But we also need range. In this case, vehicle identification, if it's a truck or a trailer, we need a certain range to read these tags, and the tags need to be reliant, specifically when they are [? mounted ?] outside the vehicle body. 我们来简要了解一下 应用实例, 以及 LF 的相关外形 因素。 在红色盒中,您可以 看到应用区域。 蓝色盒显示 主要关注的问题。 比如,我们 以牲畜和宠物为例。 这里最重要的 是可靠性。 有时,这些标准需要 在这头牛身上呆一年、两年、 甚至五年。 这个标签上的广泛范围 同样 也很重要。 同样,左边 照片中的可靠性, 我可以看到标签被 注入到鱼体内, 目的是为了给他们加上标签并 检查它们的上游迁移路径, 那么在水力发电厂 这是否仍然可以使用。 这些标签最出色的 应用是气冷蛇形盘管、铜线 和带微小芯片 或模块的天线。 玻璃封装标签 可实现完美的可靠性, 而且对于水和化学品 具有密封性能。 在汽车领域, 除可靠性外, 安全是 更重要的因素。 我们在这里看到的是 汽车防盗锁止技术。 汽车钥匙中 植入了非常微小的标签, 但同时还提供了 像 AES 密码 这样的先进安全技术。 在工业领域, 我们也将可靠性 作为关键要求。 通过稳定的 塑封标签来确保可靠性, 这类标签能够在恶劣环境下使用。 在右上角, 您看到了废物管理, 同样,可靠性 也是关键问题。 我们看到正在使用的 标签已经用了 10 年甚至 20 年,并且仍然可以正常使用。 在这种要求苛刻的非常 恶劣的环境下, 这项技术不止是 适当提供了 可靠性。 再来看看 运动领域, 所有跑过马拉松的人 都看到过鞋带上的标签。 在访问控制方面, 我们需要安全性。 但我们同样需要范围。 在这种情况下, 车辆识别, 如果是卡车或拖车, 我们需要某个范围 来读取这些标签, 而且这些标签需要 很可靠, 特别是在
Previous
下一頁
描述
2016年 8月 10日
This video highlights LF 134kHz application areas.
其他資訊
Learn more about TI solutions at TI.com
Overview of TI’s RFID and NFC portfolio
Download the NFC brochure
00:24
1
RFID Training Series Introduction
01:38
2
RFID: Decision Criteria
02:32
3
RFID: Read Range and Standards
05:07
4
RFID: Technology Characteristics
02:08
5
RFID: Coupling Examples
01:33
6
RFID: Use Cases
02:23
7
RFID: LF Applications
01:19
8
RFID: HF Applications
Related courses and events
SERIES
Near field communication (NFC)
31:48
Near Field Communication (NFC) in wearable patches...
arrow-top
close
delete
download
menu
search
sortingArrows
zoom-in
zoom-out
arrow-down
arrow-up
arrowCircle-left
arrowCircle-right
blockDiagram
calculator
calendar
chatBubble-double
chatBubble-person
chatBubble-single
checkmark-circle
chevron-down
chevron-left
chevron-right
chevron-up
chip
clipboard
close-circle
crossReference
dash
document-generic
document-pdfAcrobat
document-web
evaluationModule
globe
historyClock
info-circle
list
lock
mail
myTI
onlineDataSheet
person
phone
question-circle
referenceDesign
shoppingCart
star
tools
videos
warning
wiki