注意:各項之間請以逗號分隔

例如 , 10/17/2019

例如 , 10/17/2019

注意:各項之間請以逗號分隔

例如 , 10/17/2019

例如 , 10/17/2019

排序方式:

119 結果

TDA2 and TDA3 Processors Training Series

TI's Jacinto TDA2/TDA3 System-on-Chip (SoC) family offers scalable and open solutions based on a heterogeneous hardware and common software architecture for Advanced Driver Assistance System (ADAS) applications including camera-based front (mono/stereo), rear, surround view and night vision systems in addition to multi-range radar and sensor fusion systems. 

This training series provides an overview of the evaluation and development platforms as well as getting started with the software and development tools offered by TI on the Jacinto TDA2/TDA3 processors. 

Introduction to mmWave sensing: FMCW radars

New to mm-wave sensing? This series of five short videos provides a concise yet in-depth introduction to sensing using FMCW radars.

TI mmWave sensor device trainings

These videos describe the TI mmWave sensors and how to use them.

TI mmWave sensor labs

Labs are follow-along training videos that walk you through installation, building, and running example mmWave sensor projects.

TI mmWave Experiments: Sense the world with TI's mmWave

Sense the world with TI's mmWave is a training series where we demonstrate the capabilities of TI's IWR mmWave sensors based on questions that engineers have been asking on our mmWave sensors forum

TI mmWave sensor webinars

Take a deeper look at mmWave technology from some past webinars.

DS90UB953/954 System Design & Operation: Overview

This introduction video will give the background on FPD-Link III devices, such as the DS90UB953-Q1/ DS90UB954-Q1; the device's role within Advanced Driver Assist Systems (ADAS) in the automotive industry; and explain their broad appeal to engineers of all experience levels. This is fundamental to diving deeper into a 953/954 system, as well as, the links within the system.

DS90UB953/954 System Design & Operation: Typical Customer Issues

This section frames the design and operation video series by showing why it is important to contextualize customer problems in terms of the links between the devices. 

Specifically, this section will discuss: issues with initializing the camera and issues with reading the incorrect serializer ID from the deserializer.

DS90UB953/954 System Design & Operation: Basic Design Rules

Understanding what hardware and software settings are important is critical to establishing a foundation for the 953/954 system. These settings can occur during or after power up and may need to be changed via software. As a result, these settings are routinely checked and verified before checking any of the other links in the system.

Specifically, this sections discusses: Diagnostics post power up, Mode and IDX Pins, Clocking Modes between the 953/954, Aliasing, I2C Pass Through, Port selection on 954, Analog Launch Pad (ALP), and Successful I2C Communication

DS90UB953/954 System Design & Operation: 953-954 Link Design

This section analyzes the link between the 953 and 954 and establishes how to identify the health and operation of the link. Since the link between the 953-954 is the most fundamental link used to communicate between devices, it is often checked first.

Specifically, this section discusses: Back Channel configuration, Built in Self Test (BIST), Adaptive Equalization (AEQ), and Channel Monitor Loop (CMLOUT)

DS90UB953/954 System Design & Operation: Sensor-953 Link Design

This is the Sensor and 953 Link Design section in DS90UB953/954 System Design & Operation video series. This video discusses how to use the sensor-953 link, as well as, the specific settings that are used with this link.

DS90UB953/954 System Design & Operation: 954-ISP/SoC Link Design

This section discusses what frame synchronization (FrameSync) is and how to configure in on the 953 and 954 and how CSI2 data is transferred across the link from the 954 to the ISP/SoC

Specifically, this section discusses: Frame Synchronization (FrameSync), Controlling 953 GPIOs locally and remotely via I2C, Unsynchronized and synchronized sensors, Internal and External Frame Sync, Port Forwarding, Accessing Indirect Registers, and Pattern Generation on 953 & 954

DS90UB953/954 System Design & Operation: Hardware Design

This section discusses how design a 953/954 using Power over Coax (PoC), and various hardware checks and concepts that need to be considered when analyzing a 953/954 system.

Specifically, this section discusses: Power Over Coax (PoC), AC Coupling Capacitors, PoC Inductors, Typical PoC Schematic, Critical Signal Routing, I2C Pullups, Loop Filter Capacitors on 953, Insertion Loss, Return Loss, and Time Domain Reflection (TDR) measurements.

Introduction to FPD-Link SerDes

These introduction videos describe the evolution of FPD-Link product families, and introduction to FPD-Link III SerDes for use in Infotainment and ADAS applications.

Diagnostic & Data Protection

This video series provides an overview of diagnostic capabilities of FPD-Link III and basic tips to simplify troubleshooting.

FPD-Link Parameters & Transmission Channel

This video series describes the key parameters used in the FPD-Link high-speed serial link consisting of the serializer, transmission medium and the de-serializer.

Power over Coax (PoC)

This video series describes the concept, design and evaluation of PoC (power over coax) commonly used in ADAS sub-systems.

Interfaces

This video series describes the interfaces to sensor or video IO's of a graphics processor.

Tools

This video series describe the supporting tools for evaluating FPD-Link SerDes.

TI Automotive Seminar

德州儀器車用市場概覽

TI 在車用市場已經耕耘多年,針對175個車用系統提供各式各樣的解決方案,講師針對TI四個主要的車用技術領域說明目前市場的潮流與技術方向,包含 ADAS、車身電子與照明、車載資訊娛樂系統與儀表板,以及混合式/電氣動力系統,也以幾個具代表性的TI參考設計說明未來車用電子的發展與創新特色。
119 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki