注意:各項之間請以逗號分隔

例如 , 10/28/2021

例如 , 10/28/2021

注意:各項之間請以逗號分隔

例如 , 10/28/2021

例如 , 10/28/2021

排序方式:

9210 結果

Buck regulator architectures - voltage mode buck regulators

日期:
2013年 2月 25日

時間長度:
07:39
These presentations provide an overview of voltage mode buck regulators.

Battery charging, gauging and protection

日期:
2010年 6月 29日

時間長度:
57:21
An overview of Battery Charging, Gas Gauging and Protection solutions for single- or multi-cell battery applications, including for Li-Ion batteries

KeyStone I training: antenna Interface V2 (AIF2)

日期:
2010年 11月 9日

時間長度:
01:17:03
Antenna Interface V2 (AIF2) provides an overview of the architecture and features of AIF Version 2.

KeyStone I training: bootloader overview

日期:
2010年 11月 9日

時間長度:
20:54
This training provides an overview of the bootloader used by the KeyStone I architecture devices.

Introduction to Energy Harvesting Technology

日期:
2013年 12月 3日

時間長度:
13:56
Look at the harvesting source (solar, thermoelectric, vibration, etc.) and the transducers used with each.

KeyStone I training: debug overview

日期:
2010年 11月 9日

時間長度:
42:10
Debug Overview introduces the C66x debug features including triggers, statistics, and traces.

KeyStone I training: C66x CorePac overview - achieving high performance

日期:
2010年 10月 9日

時間長度:
31:03
CorePac: Achieving High Performance discusses how high performance can be achieved within each DSP core. Topics include CorePac architecture, Single Instruction Multiple Data (SIMD), memory access, and software pipelining.

Development Trends in Battery Technology/Chemistry

日期:
2012年 1月 1日

時間長度:
17:46
Two-part presentation on trends in baThis two-part presentations discusses current and future trends in battery technology, specifically how choices in materials affect voltages and battery capacity, e.g., modern electrolytes and the newest overlithiated layered oxides (OLO). We also take a brief look at future chemistries that offer the highest theoretical energy densities in batteries.ttery technology. How choices in materials affect voltages and battery capacity.

KeyStone I training: fast fourier transform coprocessor (FFTC)

日期:
2010年 11月 9日

時間長度:
25:22
Fast Fourier Transform Coprocessor (FFTC) presents the architecture and features of the FFT Coprocessor.

KeyStone I training: I/O interfaces

日期:
2010年 11月 9日

時間長度:
22:05
I/O Interfaces provides an overview of selected external interfaces on the C66x devices including UART, I2C, SPI, TSIP and EMIF-A.

KeyStone I training: instruction set architecture (ISA)

日期:
2015年 3月 9日

時間長度:
30:57
C66x instruction set architecture describes the differences between the TMS320C674x and the TMS320C66x instruction set included in the KeyStone CorePac.

KeyStone I training: introduction to interprocessor communication (IPC)

日期:
2010年 11月 9日

時間長度:
40:28
Introduction to Interprocessor Communication (IPC) provides an overview of the hardware and software that transports data and/or signals between threads of execution in the KeyStone family of C66x multicore devices.

KeyStone I training: memory and cache

日期:
2010年 11月 9日

時間長度:
01:01:07
C66x memory subsystem overview includes Multicore Shared Memory Controller (MSMC), local/shared memory/cache control, extended memory, and memory protection.

KeyStone I training: multicore navigator - packet DMA (PKTDMA)

日期:
2010年 11月 9日

時間長度:
32:16
Multicore Navigator: Packet DMA (PKTDMA) provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use of registers and low level drivers.

KeyStone I training: multicore navigator - queue manager subsystem (QMSS)

日期:
2010年 11月 9日

時間長度:
28:22
Multicore Navigator: Queue Manager Subsystem (QMSS) provides a detailed look at the functional elements of the QMSS and provides information on programming QMSS through the use of registers and low level drivers.

KeyStone I training: multicore navigator overview

日期:
2010年 11月 9日

時間長度:
36:36
Multicore Navigator Overview provides an introduction to the architecture and functional components of the Multicore Navigator, which includes the Queue Manager Subsystem (QMSS) and Packet DMA (PKTDMA).

KeyStone I training: multicore software development kit (MCSDK) overview

日期:
2010年 11月 9日

時間長度:
17:42
This session provides an introduction to and overview of the MCSDK.

KeyStone I training: NETCP - packet accelerator (PA)

日期:
2010年 11月 9日

時間長度:
26:36
NETCP Packet Accelerator (PA) takes a look at the motivation behind the PA, the hardware, firmware and low level drivers, as well as a programming use case.

KeyStone I training: NETCP - security accelerator (SA)

日期:
2010年 11月 9日

時間長度:
15:45
NETCP Security Accelerator (SA)takes a look at the motivation behind the SA, the firmware and low level drivers, as well as a usage case for IPSec encryption and decryption.

KeyStone I training: network coprocessor (NETCP) overview

日期:
2010年 11月 9日

時間長度:
04:20
Network Coprocessor (NETCP) Overview provides an introduction to the NETCP, which includes the Packet Accelerator (PA), Security Accelerator (SA), and Ethernet Subsystems.
9210 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki