注意:各項之間請以逗號分隔

例如 , 08/09/2022

例如 , 08/09/2022

注意:各項之間請以逗號分隔

例如 , 08/09/2022

例如 , 08/09/2022

排序方式:

24 結果
What a logic part is based on its part name. What a part name means

Anatomy of a logic part number

日期:
2018年 8月 22日

時間長度:
01:27
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.

Application specific logic

This series offers insight into a set of Logic use cases relevant to a particular group of systems and equipment.
logic bipolar inputs

Bipolar logic input operation

日期:
2021年 10月 13日

時間長度:
03:43
Learn about the structure and operation of bipolar inputs for logic devices.
Clamp diodes for logic

Clamp diodes and CMOS logic devices

日期:
2021年 10月 13日

時間長度:
02:55
Learn about clamp diodes and how they affect operation of CMOS logic devices.
Standard CMOS inputs

CMOS logic standard inputs

日期:
2021年 10月 13日

時間長度:
04:22
Learn about the operation of the input structure for standard CMOS devices.

Common applications of buffers and inverters

Learn how to overcome common challenges by utilizing logic devices to aid in optimizing system design.
Momentary switch basic schematic and bouncing waveform.

Debounce a Switch

日期:
2018年 9月 26日

時間長度:
01:42
How to debounce a switch using logic.

Dual active bridge DC:DC power stage for a level 3 (fast) EV charging station (pile)

日期:
2019年 6月 27日

時間長度:
01:04:25
Bi-directional, dual active bridge reference design for level 3 electric vehicle charging stations.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日期:
2018年 3月 28日

時間長度:
02:02
How to eliminate slow or noisy input signals.
Example signal enable circuits.

Enable or Disable a Digital Signal

日期:
2017年 11月 16日

時間長度:
02:19
How to use logic to enable or disable a signal.
Examples of systems that might need a power on reset signal.

Generate a Reset Signal at System Power On

日期:
2018年 6月 29日

時間長度:
01:13
How to generate a power on reset signal.
Some signals need to be held while the system controller is off.

Hold a Signal During Controller Reset

日期:
2018年 3月 28日

時間長度:
01:56
How to use logic to hold a signal line high or low while the system controller is powered off or held in reset.

Industry's Smallest QFN Package

日期:
2016年 9月 22日

時間長度:
04:31
Expanding the Standard Logic Products ecosystem, TI is introducing the first X1QFN package. This is the smallest QFN package available in the industry today.
Schematic representation of the internal structure for a typical open-drain buffer.

Level-shift Using Open-Drain Outputs

日期:
2018年 9月 26日

時間長度:
01:40
How to use open-drain logic devices to translate digital signals between different voltage nodes.

Logic and voltage translation

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute.
Logic ESD

Logic electrostatic discharge (ESD) protection

日期:
2021年 10月 13日

時間長度:
02:53
Learn the basics of electrostatic discharge (ESD) protection for logic devices.

Other logic

Learn more about logic and voltage translation.

Overviews of devices and EVMs

A collection of videos reviewing specific logic and voltage translation parts or EVMs, including their key features and specifications.
Schmitt-trigger CMOS inputs

Schmitt-trigger CMOS inputs

日期:
2021年 10月 13日

時間長度:
04:49
Learn about the benefits and operation of the Schmitt-trigger CMOS input architecture.

Solving Voltage Translation Solutions With One Power Rail

日期:
2015年 4月 13日

時間長度:
04:24
This video discusses applications needing voltage translation solutions with one power rail, providing examples of how to solve challenges within the design.
24 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki