Filters in use:
Filters in use:
Filters in use:
Filters in use:
Filters in use:
排序方式:
UCD3138 Digital Power Tools: Tools overview and hardware requirements
日期:
時間長度:
2016年 2月 25日
時間長度:
05:33
This video explains the software tools that TI provides for UCD3k code development and includes an introduction to the UCD3k open loop board, which is required
UCD3138 Digital Power Tools: Installing the UCD3138 device GUI
日期:
時間長度:
2016年 2月 25日
時間長度:
01:06
The UCD Device GUI is used to download firmware programs to the flash based memory on the UCD3138 family. This video demonstrates how to download and install th
UCD3138 Digital Power Tools: Source firmware - project structure and overview of lab code
日期:
時間長度:
2016年 2月 25日
時間長度:
08:36
This tutorial provides an overview of the structure of a typical UCD3138 project and examination of the source code associated.
UCD3138 Digital Power Tools: Getting started with the UCD3k device GUI
日期:
時間長度:
2016年 2月 25日
時間長度:
08:19
This video shows how the UCD device GUI can be used to write firmware to the flash based memory of the UCD3138.
UCD3138 Digital Power Tools: Boot ROM and program flash checksums
日期:
時間長度:
2016年 2月 25日
時間長度:
07:09
This video includes an overview the boot ROM program in the UCD3138, which is executed on start up. The tutorial also discusses the program flash checksums, whi
The UCD3138 Digital PWM (DPWM) Module: Introduction to the Digital PWM (DPWM) Module
日期:
時間長度:
2016年 2月 26日
時間長度:
03:59
This video introduces the three digital power peripherals, focusing on the DPWM module.
The UCD3138 Digital PWM (DPWM) Module: Setting the PWM period
日期:
時間長度:
2016年 2月 26日
時間長度:
03:58
This video shows how to set the DPWM period with firmware.
The UCD3138 Digital PWM (DPWM) Module: Controlling the DPWM outputs
日期:
時間長度:
2016年 2月 26日
時間長度:
08:30
How to write firmware to create simple waveforms on the two DPWM outputs.
The UCD3138 Digital PWM (DPWM) Module: Firmware overview and DPWM demonstration
日期:
時間長度:
2016年 2月 26日
時間長度:
04:06
This video presents lab 2 - firmware, and shows the DPWM output waveforms on an oscilloscope.
The UCD3138 Digital PWM (DPWM) Module: Memory debugger hyperknob demonstration
日期:
時間長度:
2016年 2月 26日
時間長度:
04:29
This tutorial introduces the UCD Device GUI memory debugger hyperknob, which allows modification of the DPWM output waveforms remotely via PMBus. Part of the "T
The UCD3138 Digital PWM (DPWM) Module: Solution to firmware task
日期:
時間長度:
2016年 2月 26日
時間長度:
00:29
The solution to the lab 2 firmware task. Part of the "The UCD3138 Digital PWM (DPWM) Module" series.
The UCD3138 Digital Filter Module: Introduction to the Digital Filter Module
日期:
時間長度:
2016年 2月 26日
時間長度:
05:13
This training introduces the digital filter module, which is used as the compensator in the closed loop system provided by the UCD3138 family of devices. This m
The UCD3138 Digital Filter Module: Overview of DPWM operation in normal mode
日期:
時間長度:
2016年 2月 26日
時間長度:
08:59
The previous tutorial discussed DPWM operation in open loop mode, where the PWM output was determined solely by the values of the DPWM registers.This video sho
The UCD3138 Digital Filter Module: Overview of Digital Filter architecture and operation
日期:
時間長度:
2016年 2月 26日
時間長度:
12:57
The UCD3138 filter is a PID filter with many enhancements added specifically for power supply control. In this video we discuss it's architecture and operation.
The UCD3138 Digital Filter Module: Introducing the loop mux
日期:
時間長度:
2016年 2月 26日
時間長度:
03:44
This video introduces the Loop Mux. The loop mux controls the connections between the different parts of the control loop – the Front End, the Filter, and the D
The UCD3138 Digital Filter Module: Coding tasks for this tutorial
日期:
時間長度:
2016年 2月 26日
時間長度:
03:09
This video presents the coding tasks for this tutorial, which are related to initialization of the digital filter module.
The UCD3138 Digital Filter Module: Solution to firmware tasks
日期:
時間長度:
2016年 2月 26日
時間長度:
05:56
This video presents the solution to the lab 2 firmware.
The UCD3138 Digital Filter Module: Avoiding shoot-through
日期:
時間長度:
2016年 2月 26日
時間長度:
03:22
If the rising edge of DPWMB exceeds event 4, it causes shootthrough - as both DPWMA and DPWMB are on at the same time. This could have catastrophic consequences
UCD3138 Digital Power Tools: Getting started with code composer studio
日期:
時間長度:
2016年 2月 29日
時間長度:
05:42
An overview of CCS, demonstrating how to import and build a UCD3k project.
The UCD3138 Analog Front End (AFE) Module: Introduction to the Analog Front End Module (AFE)
日期:
時間長度:
2016年 2月 29日
時間長度:
02:29
This video introduces the front end module and discusses its basic operation.