注意:各項之間請以逗號分隔

例如 , 12/09/2021

例如 , 12/09/2021

注意:各項之間請以逗號分隔

例如 , 12/09/2021

例如 , 12/09/2021

排序方式:

62 結果
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Coding tasks for this tutorial

日期:
2016年 2月 26日

時間長度:
03:09
This video presents the coding tasks for this tutorial, which are related to initialization of the digital filter module.  
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Solution to firmware tasks

日期:
2016年 2月 26日

時間長度:
05:56
This video presents the solution to the lab 2 firmware.   
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Avoiding shoot-through

日期:
2016年 2月 26日

時間長度:
03:22
If the rising edge of DPWMB exceeds event 4, it causes shootthrough - as both DPWMA and DPWMB are on at the same time. This could have catastrophic consequences
UCD3138 Digital Power Training Series

UCD3138 Digital Power Tools: Getting started with code composer studio

日期:
2016年 2月 29日

時間長度:
05:42
An overview of CCS, demonstrating how to import and build a UCD3k project.  
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Introduction to the Analog Front End Module (AFE)

日期:
2016年 2月 29日

時間長度:
02:29
This video introduces the front end module and discusses its basic operation. 
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Error ADC (EADC) Overview

日期:
2016年 2月 29日

時間長度:
06:17
This video introduces the Error Analog to Digital Converter (EADC). The EADC is the heart of the front end module.   
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Triggering the EADC

日期:
2016年 2月 29日

時間長度:
01:31
The EADC sample trigger comes from a DPWM module. This tutorial explains how to route a sample trigger from DPWM0 to Front End 0 via the loop mux. 
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: The AFE reference DAC

日期:
2016年 2月 29日

時間長度:
01:08
The front end module's reference DAC is used as the reference against which the power supply sensed feedback signal is compared. This tutorial explains how to s
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Other AFE features

日期:
2016年 2月 29日

時間長度:
02:15
Other AFE features are touched upon in this video, such as averaging the EADC output, using the front end module as a lower bandwidth and higher accuracy Succes
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Setting up the open loop board for the closed loop demo

日期:
2016年 2月 29日

時間長度:
04:11
This video shows how to setup the UCD3138 open loop board for the closed loop demonstration. This closed loop demo uses all three Digital Power Peripherals and

Setting up the open loop board for the closed loop demo

日期:
2016年 2月 29日

時間長度:
04:11
We show how to setup the UCD3138 open loop board for the closed loop demonstration. For the closed loop demo, we use all three Digital Power Peripherals and som
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Firmware overview and closed loop demo

日期:
2016年 2月 29日

時間長度:
03:24
This video explains the firmware required to create the closed loop and shows key signals on the open loop board on an oscilloscope. 
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Introduction

日期:
2016年 3月 14日

時間長度:
03:54
This video introduces the hardware and software required to communicate with the UCD3138 series of digital power controllers via JTAG. Modifications that may ne
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Installing Code Composer Studio (CCS) with JTAG support

日期:
2016年 3月 14日

時間長度:
00:59
This video demonstrates how to download and install Code Composer Studio (CCS) with JTAG support. 
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Setting up the xds10USB JTAG emulator

日期:
2016年 3月 14日

時間長度:
01:58
A once off modification that needs to be made to a file on your computer to enable JTAG comms with the UCD3138 series via the xds510USB hardware emulator is sho
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Establishing a JTAG comms link

日期:
2016年 3月 14日

時間長度:
05:06
This video will show how to establish a JTAG communications link between Code Composer Studio (CCS) and a UCD3138x device.  
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Overview of programming options

日期:
2016年 3月 14日

時間長度:
04:47
This video presents the programming options supported by the CCS JTAG flash programming GUI. Since the CCS JTAG flash GUI was designed to be as similar as possi
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Using the CCS JTAG debugger

日期:
2016年 3月 14日

時間長度:
04:59
This tutorial will show how to use the CCS JTAG debugger. Specifically, it includes how to: - run and halt the program - single step the program - view the rele
UCD3138 Digital Power Training Series

Using JTAG with the UCD3138: Exporting the contents of a CCS file via JTAG

日期:
2016年 3月 14日

時間長度:
01:49
This video demonstrates how to export the contents of flash to a file after programming. Please note that this can be a time consuming operation, so it is recom
UCD3138 Digital Power Training Series

Setting up the UCD3138 for JTAG comms

日期:
2016年 3月 14日

時間長度:
02:26
On the UCD3138, JTAG comms are disabled by default by the ROM code that executes on device startup. This video outlines the steps required to enable comms on th
62 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki