注意:各項之間請以逗號分隔

例如 , 06/26/2019

例如 , 06/26/2019

注意:各項之間請以逗號分隔

例如 , 06/26/2019

例如 , 06/26/2019

排序方式:

149 結果

KeyStone Multicore Navigator: Queue Manager Subsystem (QMSS)

日期:
2010年 11月 1日
This module provides a detailed look at the functional elements of the QMSS and provides information on programming QMSS through the use of registers and low l

KeyStone Multicore Navigator: Packet DMA

日期:
2010年 11月 1日
This module provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use

KeyStone Inter-Processor Communication (IPC)

日期:
2012年 12月 1日
This module provides an overview of the hardware and software that transports data and/or signals between threads of execution in KeyStone I C66x DSP multicore

KeyStone External Interfaces (EMIF-A, UART, I2C, SPI, TSIP)

日期:
2010年 11月 1日
This module provides an overview of selected external interfaces on KeyStone devices including UART, I2C, SPI, TSIP, and EMIF-A.

KeyStone Serial Rapid IO (SRIO)

日期:
2010年 11月 1日
This module takes a look at the new features and enhancements of the SRIO on KeyStone devices.

KeyStone FFT Co-Processor (FFTC)

日期:
2010年 11月 1日
This module presents the architecture and features of the FFT co-processor.

KeyStone Turbo Decoder Co-Processor (TCP3D)

日期:
2010年 11月 1日
This module provides an overview of TCP3D including key features, modes, drivers, and configuration. Examples are provided.

KeyStone Turbo Encoder Co-Processor (TCP3E)

日期:
2010年 11月 1日
This module provides an overview of TCP3E including usage, initialization, and configuration. Examples are provided.

Multicore Software Development Kit (MCSDK) for KeyStone Devices

日期:
2011年 10月 1日
This module provides an overview of the multicore SoC software for KeyStone I C66x DSP devices. This module introduces the optimized software components that e

KeyStone Bootloader Overview

日期:
2010年 11月 1日
This module provides an introduction to the C66x bootloader including configuration, device startup, and run-time modes.

KeyStone Power Management

日期:
2016年 6月 1日
This module provides an overview of the C66x power domain topology, power-saving features, power and clocking domains, power states, and Smart Reflex.

Save Energy with LED Lighting and Intelligent Sensing

日期:
2015年 3月 18日

時間長度:
43:58
Learn about an intelligent light which is aware of its environment and communicates to other lights using TI’s software and hardware solutions

C Compiler Tips & Tricks

日期:
2015年 3月 18日

時間長度:
58:29
Intended for those new to TI's C/C++ compiler tools. It is a collection of tips and tricks beginners find useful.

TI-RTOS Overview

日期:
2015年 5月 13日

時間長度:
32:14
This session provides an in-depth overview of TI-RTOS features

Processor SDK Overview

日期:
2015年 9月 24日
This module provides an introduction to the Processor Software Development Kit (SDK), the next generation unified software platform for TI’s newest processor fa

Introduction to Processor SDK RTOS Part 1

日期:
2015年 10月 8日
This module is the first installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It introduces the functional elements that may be included in the installation for an SoC, and then looks at these elements in more detail: TI-RTOS kernel, Inter-Processor Communication (IPC), Network Developer's Kit (NDK), algorithm libraries, and diagnostic software.

Introduction to Processor SDK RTOS Part 2

日期:
2015年 10月 8日
This module is the second installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It examines the functional elements that may be included in the installation for an SoC: Low-level Drivers (LLD), Chip Support Library (CSL), OS Abstraction Layer (OSAL), board library, Secondary Boot Loader (SBL), and board diagnostics.

Application Development Using Processor SDK RTOS

日期:
2015年 10月 8日
This presentation provides a detailed overview of the application development process using the Processor SDK RTOS release. It walks through each step of the a typical development flow, including setup of the evaluation module (EVM), getting started with the EVM, running out-of-box examples, developing application code, porting applications to custom hardware, and customization of application software.

Processor SDK Training Series

TI provides key runtime software components and documentation to further ease development. TI’s online training provides an introduction to the Processor SDK and how to use this software to start building applications on TI embedded processors.

Introduction to Digital Front End (DFE) for 66AK2L06/TCI6630K2L Processors

日期:
2015年 12月 2日
This module provides an overview of the Digital Front End (DFE) integrated into 66AK2L06/TCI6630K2L DSP + ARM processors from Texas Instruments.
149 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki