注意:各項之間請以逗號分隔

例如 , 07/20/2019

例如 , 07/20/2019

注意:各項之間請以逗號分隔

例如 , 07/20/2019

例如 , 07/20/2019

排序方式:

149 結果

Linux Board Porting Series - Module 1 - Introduction

日期:
2013年 10月 14日

時間長度:
02:28
Module 1 - Introduction: This 3-minute presentation provides an overview of "Linux Board Porting" online series. 

Linux Board Porting Series - Module 2 - Linux Board Port Overview

日期:
2015年 8月 11日

時間長度:
11:58
Module 2 - Linux Board Port Overview: Overview of the process of porting Linux and U-boot from a standard TI development platform

Linux Board Porting Series - Module 3 - Linux Boot Process

日期:
2015年 8月 24日

時間長度:
08:10
Module 3 - Linux Boot Process: Overview of the process of booting Linux on an embedded Arm Cortex device.

Linux Board Porting Series - Module 4 - Linux/U-boot Source Code Structure

日期:
2015年 8月 17日

時間長度:
11:21
Module 4 - Linux/U-boot Source Code Structure: Overview of the layered organization of the source code files for both Linux and U-boot

Linux Board Porting Series - Module 5 - Installing Code Composer Studio

日期:
2015年 8月 17日

時間長度:
09:39
Module 5 - Installing Code Composer Studio: This first lab exercise of the series is a recording of the presenter installing Code Composer Studio

Linux Board Porting Series - Module 6 - Building U-boot in CCS

日期:
2015年 8月 17日

時間長度:
08:09
Module 6 - Building U-boot in CCS: This lab exercise shows the user how to set up a makefile-based project in Code Composer Studio

Linux Board Porting Series - Module 7 - Debugging U-boot with JTAG in CCS

日期:
2015年 8月 17日

時間長度:
26:24
Module 7 - Debugging U-boot with JTAG in CCS: This module is a recording of the presenter using Code Composer Studio and an xds560 emulator to debug U-boot

Linux Board Porting Series - Module 8 - Installing SDK and Building Kernel with Debug Symbols

日期:
2015年 8月 17日

時間長度:
16:13
Module 8 - Installing SDK and Building Kernel with Debug Symbols

Linux Board Porting Series - Module 9 - Booting Linux from MMC/SD Card and TFTP

日期:
2015年 8月 17日

時間長度:
11:32
Module 9 - Booting Linux from MMC/SD Card and TFTP: This module is a recording of the presenter using the SDK utility to build a bootable MMC/SD card

Linux Board Porting Series - Module 10 - Debugging Linux Kernel with JTAG in CCS

日期:
2015年 8月 17日

時間長度:
12:27
Module 10 - Debugging Linux Kernel with JTAG in CCS: This module is a recording of the presenter configuring JTAG debugging of the Linux Kernel using CCS

KeyStone I training: antenna Interface V2 (AIF2)

日期:
2010年 11月 9日

時間長度:
01:17:03
Antenna Interface V2 (AIF2) provides an overview of the architecture and features of AIF Version 2.

KeyStone I training: bootloader overview

日期:
2010年 11月 9日

時間長度:
20:54
This training provides an overview of the bootloader used by the KeyStone I architecture devices.

KeyStone I training: debug overview

日期:
2010年 11月 9日

時間長度:
42:10
Debug Overview introduces the C66x debug features including triggers, statistics, and traces.

KeyStone I training: C66x CorePac overview - achieving high performance

日期:
2010年 10月 9日

時間長度:
31:03
CorePac: Achieving High Performance discusses how high performance can be achieved within each DSP core. Topics include CorePac architecture, Single Instruction Multiple Data (SIMD), memory access, and software pipelining.

KeyStone I training: fast fourier transform coprocessor (FFTC)

日期:
2010年 11月 9日

時間長度:
25:22
Fast Fourier Transform Coprocessor (FFTC) presents the architecture and features of the FFT Coprocessor.

KeyStone I training: I/O interfaces

日期:
2010年 11月 9日

時間長度:
22:05
I/O Interfaces provides an overview of selected external interfaces on the C66x devices including UART, I2C, SPI, TSIP and EMIF-A.

KeyStone I training: instruction set architecture (ISA)

日期:
2015年 3月 9日

時間長度:
30:57
C66x Instruction Set Architecture describes the differences between the TMS320C674x instruction set architecture and the TMS320C66x instruction set included in the KeyStone CorePac.

KeyStone I training: introduction to interprocessor communication (IPC)

日期:
2010年 11月 9日

時間長度:
40:28
Introduction to Interprocessor Communication (IPC) provides an overview of the hardware and software that transports data and/or signals between threads of execution in the KeyStone family of C66x multicore devices.

KeyStone I training: memory and cache

日期:
2010年 11月 9日

時間長度:
01:01:07
CorePac & Memory Subsystem provides a detailed look at the C66x memory subsystem including the Multicore Shared Memory Controller (MSMC), local & shared memory/cache control, extended memory, and memory protection.

KeyStone I training: multicore navigator - packet DMA (PKTDMA)

日期:
2010年 11月 9日

時間長度:
32:16
Multicore Navigator: Packet DMA (PKTDMA) provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use of registers and low level drivers.
149 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki