注意:各項之間請以逗號分隔

例如 , 01/18/2020

例如 , 01/18/2020

注意:各項之間請以逗號分隔

例如 , 01/18/2020

例如 , 01/18/2020

排序方式:

158 結果

KeyStone I C667x DSP SoC Architecture Overview

日期:
2012年 3月 1日
This module provides a high-level view of the KeyStone I C667x device architecture, the processing and memory topologies, acceleration and interface improvemen

KeyStone II DSP+ARM SoC Architecture Overview

日期:
2012年 11月 1日
This module provides a high-level view of the device architecture, including the C66x DSP and ARM Cortex-A15 processors, memory and transport topologies, netwo

KeyStone C66x DSP CorePac Overview

日期:
2012年 1月 1日
This module discusses how high performance can be achieved within each C66x DSP core. Topics include C66x DSP CorePac architecture, Single Instruction Multiple

KeyStone Instruction Set Architecture (ISA)

日期:
2011年 10月 1日
This module describes the differences between the TMS320C674x instruction set architecture and the TMS320C66x instruction set included in the KeyStone CorePac.

KeyStone Multicore Navigator

日期:
2010年 11月 1日
This module provides an introduction to the architecture and functional components of the Multicore Navigator, which includes the Queue Manager Subsystem (QMSS

KeyStone Multicore Navigator: Queue Manager Subsystem (QMSS)

日期:
2010年 11月 1日
This module provides a detailed look at the functional elements of the QMSS and provides information on programming QMSS through the use of registers and low l

KeyStone Multicore Navigator: Packet DMA

日期:
2010年 11月 1日
This module provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use

KeyStone Inter-Processor Communication (IPC)

日期:
2012年 12月 1日
This module provides an overview of the hardware and software that transports data and/or signals between threads of execution in KeyStone I C66x DSP multicore

KeyStone External Interfaces (EMIF-A, UART, I2C, SPI, TSIP)

日期:
2010年 11月 1日
This module provides an overview of selected external interfaces on KeyStone devices including UART, I2C, SPI, TSIP, and EMIF-A.

KeyStone Serial Rapid IO (SRIO)

日期:
2010年 11月 1日
This module takes a look at the new features and enhancements of the SRIO on KeyStone devices.

KeyStone FFT Co-Processor (FFTC)

日期:
2010年 11月 1日
This module presents the architecture and features of the FFT co-processor.

KeyStone Turbo Decoder Co-Processor (TCP3D)

日期:
2010年 11月 1日
This module provides an overview of TCP3D including key features, modes, drivers, and configuration. Examples are provided.

KeyStone Turbo Encoder Co-Processor (TCP3E)

日期:
2010年 11月 1日
This module provides an overview of TCP3E including usage, initialization, and configuration. Examples are provided.

Multicore Software Development Kit (MCSDK) for KeyStone Devices

日期:
2011年 10月 1日
This module provides an overview of the multicore SoC software for KeyStone I C66x DSP devices. This module introduces the optimized software components that e

KeyStone Bootloader Overview

日期:
2010年 11月 1日
This module provides an introduction to the C66x bootloader including configuration, device startup, and run-time modes.

KeyStone Power Management

日期:
2016年 6月 1日
This module provides an overview of the C66x power domain topology, power-saving features, power and clocking domains, power states, and Smart Reflex.

TI-RTOS Overview

日期:
2015年 5月 13日

時間長度:
32:14
This session provides an in-depth overview of TI-RTOS features

Processor SDK Overview

日期:
2015年 9月 24日
This module provides an introduction to the Processor Software Development Kit (SDK), the next generation unified software platform for TI’s newest processor fa

Introduction to Digital Front End (DFE) for 66AK2L06/TCI6630K2L Processors

日期:
2015年 12月 2日
This module provides an overview of the Digital Front End (DFE) integrated into 66AK2L06/TCI6630K2L DSP + ARM processors from Texas Instruments.

Leveraging DSP from Linux and RTOS: Parallel Processing and Software Support

日期:
2015年 12月 4日
This module provides an introduction to parallel processing, a programming technique that can be used to divide instructions among multiple processors
158 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki