注意:各項之間請以逗號分隔

例如 , 09/19/2019

例如 , 09/19/2019

注意:各項之間請以逗號分隔

例如 , 09/19/2019

例如 , 09/19/2019

排序方式:

159 結果

66AK2Gx Processor Training Series

Similar to existing KeyStone-based SoC devices, the 66AK2Gx enables both the DSP and ARM cores to master all memory and peripherals in the system. This architecture facilitates maximum software flexibility where either DSP- or ARM-centric system designs can be achieved. 

This curriculum provides an in-depth look at the K2G Processors, Processor SDK-Linux and TI-RTOS, and the Programmable Realtime Unit (PRU).

Application Development Using Processor SDK RTOS

日期:
2015年 10月 8日
This presentation provides a detailed overview of the application development process using the Processor SDK RTOS release. It walks through each step of the a typical development flow, including setup of the evaluation module (EVM), getting started with the EVM, running out-of-box examples, developing application code, porting applications to custom hardware, and customization of application software.

Audio System Hardware with Voice as User Interface

日期:
2017年 5月 17日

時間長度:
24:20
This training identifies the hardware components required to build an application with voice recognition capability.  

Building and Running Inter-Processor Communication (IPC) Examples on the AM572x GP EVM

日期:
2017年 12月 22日

時間長度:
04:31
This video demonstrates how to build and run Inter-Processor Communication (IPC) examples on the AM572x GP EVM using Processor SDK Linux.

C Compiler Tips & Tricks

日期:
2015年 3月 18日

時間長度:
58:29
Intended for those new to TI's C/C++ compiler tools. It is a collection of tips and tricks beginners find useful.

C55x Digital Signal Processors Software Overview

日期:
2017年 11月 21日
This module provides an overview of the software available to developers building applications on TMS320C55x Digital Signal Processors.

C55x Digital Signal Processors Training Series

TI’s TMS320C55x Fixed-Point Digital Signal Processors (DSP) enable high performance and low power through increased parallelism and total focus on power savings. Industry-leading active power enables computationally-intensive applications, such as voice triggering and encoding, to run on battery for extended period of time. Development tools include the award-winning eXpressDSP, Code Composer Studio (CCS), Integrated Development Environment (IDE), DSP/BIOS, optimized DSP and math libraries, and the industry’s largest third-party network.

C6000 Architecture (2 of 15)

日期:
2015年 4月 9日

時間長度:
01:41:39
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Cache - Lab (11 of 15)

日期:
2015年 4月 9日

時間長度:
28:59
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Cache - Overview (7 of 15)

日期:
2015年 4月 9日

時間長度:
14:29
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Cache - Part 1 (8 of 15)

日期:
2015年 4月 9日

時間長度:
22:08
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Cache - Part 2 (9 of 15)

日期:
2015年 4月 9日

時間長度:
34:10
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Cache - Part 3 (10 of 15)

日期:
2015年 4月 9日

時間長度:
46:51
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Embedded Design Workshop

This is a 15 part series covering C6000 embedded design.

C6000 Optimizations - Lab (6 of 15)

日期:
2015年 4月 9日

時間長度:
01:23:28
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Optimizations - Overview (3 of 15)

日期:
2015年 4月 9日

時間長度:
29:23
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Optimizations - Part 1 (4 of 15)

日期:
2015年 4月 9日

時間長度:
01:09:30
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

C6000 Optimizations - Part 2 (5 of 15)

日期:
2015年 4月 9日

時間長度:
01:01:04
This training series provides an in-depth look at C6000 architecture such as cache, using the C compiler/optimizer, EDMA3 and a great intro to the architecture

Debugging Common Application Issues with TI-RTOS

日期:
2016年 5月 25日

時間長度:
25:26
This presentation shows how TI-RTOS helps a user debug the following common application issues: stack overflows, device exceptions, and memory mismanagement.

Debugging Embedded Linux Systems Training Series

Linux is well-adopted within embedded systems. But debugging Linux system issues can be overwhelming. This training series teaches the techniques of debugging kernel issues that may be encountered in embedded Linux systems. This training series explains the Linux kernel logging system and logging API, illustrates how to locate a particular device driver, and demonstrates how to read kernel oops logs.

159 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki