注意:各項之間請以逗號分隔

例如 , 06/28/2022

例如 , 06/28/2022

注意:各項之間請以逗號分隔

例如 , 06/28/2022

例如 , 06/28/2022

排序方式:

79 結果
schematic for R-S Latch driving an LED

Design an Alarm / Tamper Circuit with an S-R Latch

日期:
2018年 9月 27日

時間長度:
02:26
How to use NOR/NAND gates to create an S-R Latch for Alarm circuits
Schematic representation of an xor gate inputs and output

Detect Phase Differences in Input Signals

日期:
2018年 9月 28日

時間長度:
01:09
How to use logic to detect a phase difference in input signals.

Discrete Level Translation Replacement

日期:
2018年 5月 23日

時間長度:
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
03:18
A deep look at how an LSF device achieves down translation.

Dual active bridge DC:DC power stage for a level 3 (fast) EV charging station (pile)

日期:
2019年 6月 27日

時間長度:
01:04:25
Bi-directional, dual active bridge reference design for level 3 electric vehicle charging stations.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日期:
2018年 3月 28日

時間長度:
02:02
How to eliminate slow or noisy input signals.
Example signal enable circuits.

Enable or Disable a Digital Signal

日期:
2017年 11月 16日

時間長度:
02:19
How to use logic to enable or disable a signal.

Enabling Image Sensor to Process Interfaces with Level Translation

日期:
2018年 12月 21日

時間長度:
04:15
Enabling IP camera image sensor to processor interfaces with voltage translation
Examples of systems that might need a power on reset signal.

Generate a Reset Signal at System Power On

日期:
2018年 6月 29日

時間長度:
01:13
How to generate a power on reset signal.
Some signals need to be held while the system controller is off.

Hold a Signal During Controller Reset

日期:
2018年 3月 28日

時間長度:
01:56
How to use logic to hold a signal line high or low while the system controller is powered off or held in reset.
Schematic representation of GPIO Input Expansion

Increase the Number of Inputs on a Microcontroller

日期:
2019年 8月 21日

時間長度:
01:33
How to use a shift register to expand the input capacity of your microcontroller. (GPIO Input Expansion)

Increase the number of outputs on a microcontroller

日期:
2019年 9月 20日

時間長度:
01:44
How to use a Serial In Parallel Out (SIPO) shift register to increase the number of outputs on your microcontroller (GPIO Output Expansion).

Industry's Smallest QFN Package

日期:
2016年 9月 22日

時間長度:
04:31
Expanding the Standard Logic Products ecosystem, TI is introducing the first X1QFN package. This is the smallest QFN package available in the industry today.
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日期:
2018年 5月 21日

時間長度:
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.
Introduction to the SN74AXCH4T245 four bit voltage level translator

Introducing the SN74AXCH4T245 4-bit low voltage direction controlled level translator with bus hold

日期:
2019年 4月 4日

時間長度:
03:49
Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introducing the SN74AXCH8T245 8-bit direction controlled level translator with bus hold

日期:
2018年 9月 14日

時間長度:
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.

Introduction to the AXC family of direction controlled translation device

日期:
2017年 11月 7日

時間長度:
03:57
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXC1T45.
Introduction to the SN74AXC2T45 two channel voltage level translator

Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator

日期:
2019年 4月 30日

時間長度:
03:06
Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator
Introduction to the SN74AXC4T245 four bit voltage level translator

Introduction to the SN74AXC4T245 four bit low voltage direction controlled level translator

日期:
2018年 12月 21日

時間長度:
03:03
Key features and benefits of the SN74AXC4T245 four bit low voltage direction controlled level translator
sn74axc4t774

Introduction to the SN74AXC4T774

日期:
2019年 7月 5日

時間長度:
03:22
Learn about the key features and benefits of the SN74AXC4T774 four bit low voltage direction controlled level translator.
79 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki