注意:各項之間請以逗號分隔

例如 , 12/02/2021

例如 , 12/02/2021

注意:各項之間請以逗號分隔

例如 , 12/02/2021

例如 , 12/02/2021

排序方式:

79 結果
Pitfalls of Discrete Push-Pull Level Shifting

Understanding the pitfalls of discrete level shifting circuits

日期:
2018年 5月 21日

時間長度:
08:23
This video outlines common drawbacks to discrete push-pull level shifting implementations, introducing the 2N7001T device as a discrete replacement.

Discrete Level Translation Replacement

日期:
2018年 5月 23日

時間長度:
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Automotive Current Shunt Monitoring

Automotive Current Monitoring Using High Speed Amplifiers

日期:
2018年 5月 24日

時間長度:
05:11
Automotive Current Monitoring Using High Speed Amplifiers

Logic and voltage translation

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute.
Schematic representation of matching inverted clock inputs with an inverter.

Synchronize Inverted Clock Inputs

日期:
2018年 6月 29日

時間長度:
01:04
How to synchronize devices with inverted clock inputs operating off the same clock source.
Examples of systems that might need a power on reset signal.

Generate a Reset Signal at System Power On

日期:
2018年 6月 29日

時間長度:
01:13
How to generate a power on reset signal.
What a logic part is based on its part name. What a part name means

Anatomy of a logic part number

日期:
2018年 8月 22日

時間長度:
01:27
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.
Understanding Bus Hold Functionality for Level Translators

Understanding Bus Hold Functionality for Level Translators

日期:
2018年 9月 8日

時間長度:
02:32
This video provides an overview of the bus hold functionality found on many level translators and its suitability for use within applications.
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introducing the SN74AXCH8T245 8-bit direction controlled level translator with bus hold

日期:
2018年 9月 14日

時間長度:
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.
Schematic representation of a D-Type Flip-Flop to toggle a system on or off using a momentary switch.

Convert a Momentary Switch to a Toggle Switch

日期:
2018年 9月 11日

時間長度:
01:31
How to use logic to utilize a momentary switch in place of a toggle switch.
Momentary switch basic schematic and bouncing waveform.

Debounce a Switch

日期:
2018年 9月 26日

時間長度:
01:42
How to debounce a switch using logic.
Schematic representation of the internal structure for a typical open-drain buffer.

Level-shift Using Open-Drain Outputs

日期:
2018年 9月 26日

時間長度:
01:40
How to use open-drain logic devices to translate digital signals between different voltage nodes.
schematic for R-S Latch driving an LED

Design an Alarm / Tamper Circuit with an S-R Latch

日期:
2018年 9月 27日

時間長度:
02:26
How to use NOR/NAND gates to create an S-R Latch for Alarm circuits
Schematic representation of an xor gate inputs and output

Detect Phase Differences in Input Signals

日期:
2018年 9月 28日

時間長度:
01:09
How to use logic to detect a phase difference in input signals.

Translation Between Communication Modules and System Controllers

日期:
2018年 11月 5日

時間長度:
01:37
How to choose the correct auto bidirectional translator for communication modules and system controllers.

Enabling Image Sensor to Process Interfaces with Level Translation

日期:
2018年 12月 21日

時間長度:
04:15
Enabling IP camera image sensor to processor interfaces with voltage translation
Introduction to the SN74AXC4T245 four bit voltage level translator

Introduction to the SN74AXC4T245 four bit low voltage direction controlled level translator

日期:
2018年 12月 21日

時間長度:
03:03
Key features and benefits of the SN74AXC4T245 four bit low voltage direction controlled level translator
UART interface

Voltage Level Translation for UART Interface

日期:
2019年 1月 1日

時間長度:
02:27
TI's signal level translation for the UART interface

Voltage translation in switches and routers

日期:
2019年 2月 21日

時間長度:
01:57
Next-generation switches and routers are using lower operating voltages in their systems; creating the need for voltage translation to solve voltage mismatches.
Introduction to the SN74AXCH4T245 four bit voltage level translator

Introducing the SN74AXCH4T245 4-bit low voltage direction controlled level translator with bus hold

日期:
2019年 4月 4日

時間長度:
03:49
Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator
79 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki