注意:各項之間請以逗號分隔

例如 , 09/18/2019

例如 , 09/18/2019

注意:各項之間請以逗號分隔

例如 , 09/18/2019

例如 , 09/18/2019

排序方式:

30 結果
What a logic part is based on its part name. What a part name means

Anatomy of a Logic Part Number

日期:
2018年 8月 22日

時間長度:
01:34
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.

Choosing the right auto bidirectional voltage translator

日期:
2019年 7月 5日

時間長度:
02:36
How to decide which family of auto bidirectional voltage translators to use.

Discrete Level Translation Replacement

日期:
2018年 5月 23日

時間長度:
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
03:19
A deep look at how an LSF device achieves down translation.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日期:
2018年 3月 28日

時間長度:
02:02
How to eliminate slow or noisy input signals.

Enabling Image Sensor to Process Interfaces with Level Translation

日期:
2018年 12月 21日

時間長度:
04:15
Enabling IP camera image sensor to processor interfaces with voltage translation
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日期:
2018年 5月 21日

時間長度:
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.
Introduction to the SN74AXC2T45 two channel voltage level translator

Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator

日期:
2019年 4月 30日

時間長度:
03:06
Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator
Introduction to the SN74AXC4T245 four bit voltage level translator

Introduction to the SN74AXC4T245 four bit low voltage direction controlled level translator

日期:
2018年 12月 21日

時間長度:
03:03
Key features and benefits of the SN74AXC4T245 four bit low voltage direction controlled level translator
sn74axc4t774

Introduction to the SN74AXC4T774

日期:
2019年 7月 5日

時間長度:
03:22
Learn about the key features and benefits of the SN74AXC4T774 four bit low voltage direction controlled level translator.
Introduction to the SN74AXCH4T245 four bit voltage level translator

Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator with bus hold

日期:
2019年 4月 4日

時間長度:
03:49
Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introduction to the SN74AXCH8T245 eight bit direction controlled level translator with bus hold functionality

日期:
2018年 9月 14日

時間長度:
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.
Schematic representations for each LSF device in the family

Introduction – Voltage Level Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
01:25
Introduction to the LSF video series and the LSF family of devices

Logic and Voltage Translation Videos

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute, the technical video series created by the experts on logic and voltage translation devices.

Multi-voltage translation schematic for the LSF family of devices.

Multi-voltage Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:56
How to use a single LSF device to translate between multiple voltages in the same system.

Signal Level Translation

日期:
2018年 5月 3日

時間長度:
02:03
Level translation for standard Interfaces
Single supply translation schematic for the LSF family of devices.

Single Supply Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:12
How to use the LSF when there are supply limitations.

Solving Voltage Translation Solutions With One Power Rail

日期:
2015年 4月 13日

時間長度:
04:24
This video discusses applications needing voltage translation solutions with one power rail, providing examples of how to solve challenges within the design.
SPI level translation AXC4T774 EVM

SPI JTAG Level translation using AXC4T774EVM

日期:
2019年 7月 5日

時間長度:
04:29
Low voltage level translation using SN74AXC4T774EVM

The Logic Minute – Logic and Translation

The Logic Minute video series make complex ideas related to logic and translation easy to understand in just a couple minutes. 

30 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki