注意:各項之間請以逗號分隔

例如 , 06/23/2022

例如 , 06/23/2022

注意:各項之間請以逗號分隔

例如 , 06/23/2022

例如 , 06/23/2022

排序方式:

46 結果

Solving Voltage Translation Solutions With One Power Rail

日期:
2015年 4月 13日

時間長度:
04:24
This video discusses applications needing voltage translation solutions with one power rail, providing examples of how to solve challenges within the design.
Schematic representations for each LSF device in the family

Introduction – Voltage Level Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
01:25
Introduction to the LSF video series and the LSF family of devices
Internal schematic for LSF bias circuit operation

Understanding the Bias Circuit for the LSF Family

日期:
2017年 10月 17日

時間長度:
03:20
A deep look at how the bias circuit works in an LSF device.
Example incorrect circuit for the enable pin of the LSF.

Using the Enable Pin with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:25
How to use the enable pin correctly with an LSF device.
Simplified translation schematic with the LSF.

Translation Basics with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:35
An overview of translation concepts and terms common to the down translation and up translation videos.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
03:18
A deep look at how an LSF device achieves down translation.
Internal schematic for up translation with an LSF family device.

Up Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
05:39
A deep look at how an LSF device achieves up translation.
Multi-voltage translation schematic for the LSF family of devices.

Multi-voltage Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:56
How to use a single LSF device to translate between multiple voltages in the same system.
Single supply translation schematic for the LSF family of devices.

Single Supply Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:12
How to use the LSF when there are supply limitations.

The Logic Minute – Logic and translation

The Logic Minute video series makes complex ideas related to logic and translation easy to understand in just a couple of minutes.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日期:
2018年 3月 28日

時間長度:
02:02
How to eliminate slow or noisy input signals.

Signal Level Translation

日期:
2018年 5月 3日

時間長度:
02:03
Level translation for standard Interfaces
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日期:
2018年 5月 21日

時間長度:
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.
Pitfalls of Discrete Push-Pull Level Shifting

Understanding the pitfalls of discrete level shifting circuits

日期:
2018年 5月 21日

時間長度:
08:23
This video outlines common drawbacks to discrete push-pull level shifting implementations, introducing the 2N7001T device as a discrete replacement.

Discrete Level Translation Replacement

日期:
2018年 5月 23日

時間長度:
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.

Logic and voltage translation

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute.
What a logic part is based on its part name. What a part name means

Anatomy of a logic part number

日期:
2018年 8月 22日

時間長度:
01:27
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.
Understanding Bus Hold Functionality for Level Translators

Understanding Bus Hold Functionality for Level Translators

日期:
2018年 9月 8日

時間長度:
02:32
This video provides an overview of the bus hold functionality found on many level translators and its suitability for use within applications.
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introducing the SN74AXCH8T245 8-bit direction controlled level translator with bus hold

日期:
2018年 9月 14日

時間長度:
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.

Translation Between Communication Modules and System Controllers

日期:
2018年 11月 5日

時間長度:
01:37
How to choose the correct auto bidirectional translator for communication modules and system controllers.
46 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki