注意:各項之間請以逗號分隔

例如 , 12/03/2021

例如 , 12/03/2021

注意:各項之間請以逗號分隔

例如 , 12/03/2021

例如 , 12/03/2021

排序方式:

46 結果

Enabling Image Sensor to Process Interfaces with Level Translation

日期:
2018年 12月 21日

時間長度:
04:15
Enabling IP camera image sensor to processor interfaces with voltage translation
Introduction to the SN74AXC4T245 four bit voltage level translator

Introduction to the SN74AXC4T245 four bit low voltage direction controlled level translator

日期:
2018年 12月 21日

時間長度:
03:03
Key features and benefits of the SN74AXC4T245 four bit low voltage direction controlled level translator

Translation Between Communication Modules and System Controllers

日期:
2018年 11月 5日

時間長度:
01:37
How to choose the correct auto bidirectional translator for communication modules and system controllers.
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introducing the SN74AXCH8T245 8-bit direction controlled level translator with bus hold

日期:
2018年 9月 14日

時間長度:
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.
Understanding Bus Hold Functionality for Level Translators

Understanding Bus Hold Functionality for Level Translators

日期:
2018年 9月 8日

時間長度:
02:32
This video provides an overview of the bus hold functionality found on many level translators and its suitability for use within applications.
What a logic part is based on its part name. What a part name means

Anatomy of a logic part number

日期:
2018年 8月 22日

時間長度:
01:27
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.

Logic and voltage translation

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute.

Discrete Level Translation Replacement

日期:
2018年 5月 23日

時間長度:
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Pitfalls of Discrete Push-Pull Level Shifting

Understanding the pitfalls of discrete level shifting circuits

日期:
2018年 5月 21日

時間長度:
08:23
This video outlines common drawbacks to discrete push-pull level shifting implementations, introducing the 2N7001T device as a discrete replacement.
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日期:
2018年 5月 21日

時間長度:
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.

Signal Level Translation

日期:
2018年 5月 3日

時間長度:
02:03
Level translation for standard Interfaces
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日期:
2018年 3月 28日

時間長度:
02:02
How to eliminate slow or noisy input signals.

Low Voltage Translation using SN74AXC8T245

日期:
2018年 2月 21日

時間長度:
04:09
This video introduces the industry's low voltage translator, SN74AXC8T245 along with an application to demonstrate the translation using the SN74AXC8T245EVM

Introduction to the AXC family of direction controlled translation device

日期:
2017年 11月 7日

時間長度:
03:57
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXC1T45.

The Logic Minute – Logic and translation

The Logic Minute video series makes complex ideas related to logic and translation easy to understand in just a couple of minutes.
Multi-voltage translation schematic for the LSF family of devices.

Multi-voltage Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:56
How to use a single LSF device to translate between multiple voltages in the same system.
Single supply translation schematic for the LSF family of devices.

Single Supply Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:12
How to use the LSF when there are supply limitations.
Internal schematic for up translation with an LSF family device.

Up Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
05:39
A deep look at how an LSF device achieves up translation.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日期:
2017年 10月 17日

時間長度:
03:18
A deep look at how an LSF device achieves down translation.
Simplified translation schematic with the LSF.

Translation Basics with the LSF Family

日期:
2017年 10月 17日

時間長度:
02:35
An overview of translation concepts and terms common to the down translation and up translation videos.
46 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki